Technical FAQs

Ask a Question

What does ``1 way horizontal `` mean in relation to an XCKP121?

The cam or target moves horizontally and hits the roller actuator from one direction to operate the switch. An example of this can be seen on digest 172 page 19-28 in the XCKML121 switch. Once the cam has cleared the roller and the roller has returned to its initial position, a cam travelling in the opposite direction will not actuate the mechansim and the contacts will not change state for movement of the cam in this opposite direction.

CTA-ID : 2007834
Was this helpful?
What can we do to improve the information ?