Technical FAQs

Ask a Question

Can a shunt trip accessory be added to the main breaker of the EZM1600CB Series M01?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Accessories

Cause:
Application

Resolution:

Yes. The main breaker used in the EZM1600CB Series M01, is the MHP26600. The MA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are MA11042 (24 Vac), MA11037 (277 or 480 Vac), MA11027 (24 Vdc), MA11028 (48 Vdc), MA11029 (125 Vdc) and MA11030 (250 Vdc).


 
Was this helpful?
What can we do to improve the information ?