Technical FAQs

Ask a Question

What are the repair parts for a QMJ366, Series E1 (E01)?

Only the parts listed below are considered field replaceable:

Arc Suppressor Assembly (3 per switch) - 40520-318-50
Load Base Assembly (3 per switch, includes lugs) - 40521-120-50
Handle Knob Kit - 40283-435-50
Lug Assembly (per lug) - 40251-287-50
Lug Mounting nut (per lug) - 23427-024-00
Load Base Mounting Screw (3 required per load base) - 21427-202-41


CTA-ID : 2007882
Was this helpful?
What can we do to improve the information ?