Technical FAQs

Ask a Question

Can a shunt trip accessory be added to an EZM1400CBU?

Yes. The main breaker used is the LHF26400. The LA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are LA11042 (24 Vac), LA11037 (277 or 480 Vac), LA11027 (24 Vdc), LA11028 (48 Vdc), LA11029 (125 Vdc) and LA11030 (250 Vdc).

CTA-ID : 2007879
Was this helpful?
What can we do to improve the information ?