Technical FAQs

Ask a Question

Can a shunt trip accessory be added to an EZM1400CB?

Issue:
Product design features

Product Line:
EZM Metering

Environment:
Shunt Trip

Cause;
Application

Resolution:
Yes. The main breaker used is the LHP26400. The LA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are LA11042 (24 Vac), LA11037 (277 or 480 Vac), LA11027 (24 Vdc), LA11028 (48 Vdc), LA11029 (125 Vdc) and LA11030 (250 Vdc).


CTA-ID : 2007881
Was this helpful?
What can we do to improve the information ?