Technical FAQs

Ask a Question

What is the ``Test`` feature on the GS1AHT110/120/130/140 and the GS1AHT410/420/430/440 switch/handle?

The ``Test`` position enables the testing of the control circuit auxiliaries without switching the main contacts or removing the fuses. This function provides an alternative to a separately wired push to test button.

CTA-ID : 2008538
Was this helpful?
What can we do to improve the information ?