Technical FAQs

Ask a Question

Are optional lugs available for Heavy Duty safety switches?


Product Line:
Heavy Duty Safety Switch

Selection of optional lugs

Copper only lugs and crimp type lugs may be available for some, but not all, Heavy Duty safety switches. Consult the latest Square D Digest, or Digest Plus Selector (on-line at, for selection. Lugs to extend the wire range or to multiply the number of conductors are not available.

The exception is the 200A Heavy Duty Safety Switches. Optional Lug Kit AL20DTF will accept up to (2) #6 AWG - 300 KCMIL AL or CU wires. The maximum wire bending space available allows for 250 KCMIL maximum wires.

NOTE: The AL20DTF is NOT a UL listed kit and will not be noted on the 200A Heavy Duty Safety Switch wiring diagrams as a listed accessory. 

CTA-ID : 2008533
Was this helpful?
What can we do to improve the information ?