Technical FAQs

Ask a Question

Can I install a cover-mounted control Stop/Start push button kit in a 9991DPG1 enclosure?

No, the kit requires a NEMA starter and will not work on a 9991 DPG1. Also, there is no knockout for the kit. The user must use a separate control station.


CTA-ID : 2008080
Was this helpful?
What can we do to improve the information ?