Technical FAQs

Ask a Question

What are the repair parts for a QMJ364H, Series E1 (E01)?

This QMJ device is only a single switch and it cannot be modified in the field to add an additional switch. Parts are listed per switch. Only the parts listed below are considered field replaceable:
-Arc Shield/Suppressor Assembly (1 each required) - 40520-214-50 (Arc Suppressor Housing) and 40520-173-02 (Arc Shield)
-Load Base Assembly (1 required, does not include lugs, fuse connector assembly) - 40521-070-50
-Fuse connector assembly - 40521-076-50 (one required per phase)
-Fuse mounting nuts(3 per fuse connector) - 23427-020-01
-Lug Assembly (per lug) - 40251-162-51
-Lug mounting nut - 23427-022-00
-Load base mounting screw - 40205-065-01
-Handle Knob Kit - 40283-437-50

CTA-ID : 2007869
Was this helpful?
What can we do to improve the information ?