Technical FAQs

Ask a Question

What is the AIR rating of the KC/KCL34225 breaker?

It is 65,000A RMS at 480V and 100,000A RMS at 240V.


CTA-ID : 2008531
Was this helpful?
What can we do to improve the information ?