Technical FAQs

Ask a Question

CK800---what is the temperature rise on the terminals?

UL489 states that the temperature on the terminal shall not exceed a 50 degree C rise above the ambient temperature (40 degree C).


CTA-ID : 2008525
Was this helpful?
What can we do to improve the information ?