Technical FAQs

Ask a Question

What is the UL amperage rating of the 9421 V1G30 switch?

The amperage rating is 20A UL, and 32A IEC.


CTA-ID : 2008522
Was this helpful?
What can we do to improve the information ?