Technical FAQs

Ask a Question

What are the repair parts for a QMJ361T, Series E1 (E01)?

This QMJ device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 40512-534-50
Load Base Assembly (1 required, includes lugs) - 4056002550K
Handle Knob Kit - 40283-437-50
Lug Assembly (per lug) - 40251-016-52
Lug mounting screw - 21963-171-80
load base mounting screw 21427-171-61

CTA-ID : 2007865
Was this helpful?
What can we do to improve the information ?