Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H322NRB, Series F05 Heavy Duty safety switch?

The lugs on this device will accept (1) #12 - 2 AWG aluminum or (1) #14 - 2 AWG copper conductor per phase. However, wire bending space available in the switch restricts the conductors to (1) #3 AWG maximum.

CTA-ID : 2008513
Was this helpful?
What can we do to improve the information ?