Technical FAQs

Ask a Question

What is the thread size for XVBC11?

Issue:
What is the thread size for  XVBC11?

Product Line:
Harmony Tower Lights

Environment:
All Products

Cause:
Product Features

Resolution:
This has metric threads that are M23 x 1.5, 10mm is total length of threads.


CTA-ID : 2008275
Was this helpful?
What can we do to improve the information ?