Technical FAQs

Ask a Question

What is the wire range of an LA9D2561 ?

It is the same as for the LC1D25: (1) # 16 - # 8 AWG or (2) # 16 - # 10 AWG.


CTA-ID : 2008049
Was this helpful?
What can we do to improve the information ?