Technical FAQs

Ask a Question

Are Square D Heavy Duty safety switches available for use in a hazardous location environment?

Square D does not offer a Visible-Blade type of Heavy Duty disconnect in Hazardous Location (NEMA 7 or NEMA 9) enclosures. For a not-fusible applications, we offer enclosed automatic molded case switches. Where overcurrent and short circuit protection is required, we offer Hazardous Location enclosures for molded case circuit breakers.

CTA-ID : 2008044
Was this helpful?
What can we do to improve the information ?