Technical FAQs

Ask a Question

Are Square D Double Throw safety switches available for use in a corrosive environment?

Issue:
Product Design Features

Product Line:
Double throw safey switches

Environement:
NEMA enclosure ratings

Cause:
Application

Resolution:
ALL 
Square D Double Throw safety switches have specific NEMA ratings for the enclosures and some of them are available in NEMA 4X enclosures. The NEMA 4X enclosures are manufactured from Type 304 stainless steel, but NOT all voltage/current ratings are available in NEMA 4X. Please see the current on-line digest or contact a local authorized Square D/SE distributor for products available for this application.


CTA-ID : 2008042
Was this helpful?
What can we do to improve the information ?