Technical FAQs

Ask a Question

Is it possible to remove the trip unit from an NS600N breaker in these in field to convert its operation to a disconnect switch only with no overcurrent protection?

No. There is no way to make an NS circuit breaker into a switch. The switch has no CT, and no trip unit has been developed to make this conversion.

CTA-ID : 2007836
Was this helpful?
What can we do to improve the information ?