Technical FAQs

Ask a Question

Will the hand held test kit for the Micrologic 2.0 series and the compact STR trip units also work on the STR 58U trip unit? In the instruction bulletin it showes it only going up to STR 53.

The handheld (S33594) and full function (S33595) test kit will not test the STR58U used on the MP style Masterpact. The ME test kit, part number 55391, is required.

CTA-ID : 2007831
Was this helpful?
What can we do to improve the information ?