Technical FAQs

Ask a Question

Does the PL breaker have a 50kA 600Vac rating?

No, the PL is only rated for 25 kAIC at 600 V. However, the PK breaker has the following UL ratings: 65kA at 240Vac and 480Vac, 50kA at 600Vac. This breaker is marketed in Canada and is available in the USA and has UL, CSA and IEC ratings.

CTA-ID : 2008259
Was this helpful?
What can we do to improve the information ?