Technical FAQs

Ask a Question

Is it possible to field install a main breaker in an Iline panelboard?

Issue:
Is it possible to field install a main breaker in an Iline panelboard?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Only as a back-fed main provided the interior is the correct size and has enough branch mounting space available to accept the breaker.


CTA-ID : 2007822
Was this helpful?
What can we do to improve the information ?