Technical FAQs

Ask a Question

Is the Square D E50 overload heater the same as Furnas E50 overload heater?

Yes, the 8536 NEMA size 3 and 4 devices with bi-metallic overload relays do use the Furnas type overload block and heaters.

CTA-ID : 2007816
Was this helpful?
What can we do to improve the information ?