Technical FAQs

Ask a Question

9038 CG**: What replaces operating lever, part number 65079-042-01, which is shown on the service bulletin but is not system recognized.

Part no. 65079-042-01 is replaced by:
lever 2810C4X2
screw 21911-14161







CTA-ID : 2007264
Was this helpful?
What can we do to improve the information ?