Technical FAQs

Ask a Question

Can I use a TVS4EMA on a single phase application? Two legs and a neutral.

That is a 480/277V 3 phase unit. John at TVSS tag says that the alarm will sound if one of the phases is not hooked up. Best solution is to double up one of the phases to ``fool`` the alarm into not sounding, taking care of the diagnostic issue.


CTA-ID : 2007807
Was this helpful?
What can we do to improve the information ?