Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a HU362AWC safety switch?

Ground lugs (2) are provided factory installed in the HU362AWC (Series F01 - F07 design). The lugs will each accept (1) #14 - 8 AWG solid copper conductor or (1) #14 - 4 AWG stranded copper conductor (Series F01 - F06). The lugs will each accept (1) #14 - 2 AWG aluminum or (1) #12 - 2 copper conductor (Series F07).


CTA-ID : 2005437
Was this helpful?
What can we do to improve the information ?