Technical FAQs

Ask a Question

What are the AIR ratings for a thermal-mag LA-MC & LH-MC breakers ?

These ``mission critical `` breakers are rated at 30k and 35kaic 480v max


CTA-ID : 2008228
Was this helpful?
What can we do to improve the information ?