Technical FAQs

Ask a Question

What is the maximum ampere settings for the ground fault on the Square D Series B micrologic breakers?

The ground fault ampere setting can be adjusted from 0.2 to 0.75 of the sensor rating of breakers up through 1600A sensor sizes For 2000A sensors and higher, the maximum setting is 1200A.

CTA-ID : 2008002
Was this helpful?
What can we do to improve the information ?