Technical FAQs

Ask a Question

What Tenant Circuit Breakers were used with a EZM742200R Meter Center?

Issue:
Product Design Features

Product Line:
EZ Metering Equipment

Environment:
Tenant breakers

Cause:
Application/Installation

Resolution:

This obsolete EZM Meter Center used EH (60 ampere) or QE-VH (70 through 200 ampere), tenant circuit breakers.


CTA-ID : 2007788
Was this helpful?
What can we do to improve the information ?