Technical FAQs

Ask a Question

What Tenant Circuit Breakers were used with the Old Style EZM743200R EZM branch device?

Issue:
Previous design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Issue:
Maintenance

Resolution:
The old style EZM743200R branch device is obsolete and used the EH (60 ampere) or QE-VH (70 through 200 ampere), tenant circuit breakers. The EH and QE-VH tenant breakers are obsolete, no longer available with NO replacements.


CTA-ID : 2007789
Was this helpful?
What can we do to improve the information ?