Technical FAQs

Ask a Question

What Tenant Circuit Breakers were used with the OLD EZM744200R EZM branch device?

Issue:
Previous design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Issue:
Maintenance

Resolution:
The EZM744200R is an obsolete EZM Metering branch device that used EH (60 ampere) or QE-VH (70 through 200 ampere), tenant circuit breakers. The EH and QE tenant breakers are Obsolete, no longer available with NO replacements



CTA-ID : 2007790
Was this helpful?
What can we do to improve the information ?