Technical FAQs

Ask a Question

What Tenant Circuit Breakers were used with a EZM744200MR Meter Center?

Issue:
Old Product Design Features

Product Line:
EZM Metering Equipment

Cause:
Installation

Resolution:
This obsolete EZM Meter Center used EH (60 ampere) or QE-VH (70 through 200 ampere), tenant circuit breakers. But the EH and QE tenant breakers are Obsolete, NLA with no replacements.

 
Was this helpful?
What can we do to improve the information ?