Technical FAQs

Ask a Question

What Tenant Circuit Breakers were used with the Old style EZM741200R EZM Branch Device?

Issue:
Previous design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Issue:
Maintenance

Resolution:
The EZM741200R is an obsolete EZM Metering branch device that used EH (60 ampere) or QE-VH (70 through 200 ampere), tenant circuit breakers. The EH and QE tenant breakers are Obsolete, no longer available with NO replacements


CTA-ID : 2007787
Was this helpful?
What can we do to improve the information ?