Technical FAQs

Ask a Question

What is the difference between the HU361AWK and the HU3612AWK?

Issue:
Product Features

Product Line:
HD SS

Cause:
Product Features

Resolution:
The HU361AWK is a 30 Ampere switch that is provided in the standard 30 Ampere size of enclosure. The HU3612AWK is a 30 Ampere switch that is provided in 60 Ampere size of enclosure.


CTA-ID : 2007978
Was this helpful?
What can we do to improve the information ?