Technical FAQs

Ask a Question

Can a QO330MQ125, Series S03, load center be top or bottom fed?

This load center is provided with the main circuit breaker positioned at the top for a top feed application. It can be modified in the field for bottom main breaker positioning. First, rotate the main breaker 180 degrees, then rotate the entire load center 180 degrees.

CTA-ID : 2008184
Was this helpful?
What can we do to improve the information ?