Technical FAQs

Ask a Question

What is the range of voltage that can be applied to QO120GFI?

The voltage range is 85% to 110% per UL standards.


CTA-ID : 2008634
Was this helpful?
What can we do to improve the information ?