Technical FAQs

Ask a Question

Can you mount a Square D Mini Power Zone on a pedestal?

Issue:
Can you mount a Square D Mini Power Zone on a pedestal?

Product Line:
LV Transformers.

Environment:
Products sold in the United States.

Cause:
Assembly/Installation

Resolution:
The Mini Power Zone (MPZ) can be mounted on a pedestal as long as the pedestal will support the weight of the Mini Powerzone and provided the ``pedestal`` is designed to emulate a wall mount method. Thus the ``pedestal`` would have vertical runners up the back side of the MPZ such that it`s weight is supported via it`s designed wall mounting method..


CTA-ID : 2008178
Was this helpful?
What can we do to improve the information ?