Technical FAQs

Ask a Question

Why are Multi-9 C60N breakers rated for 480/277V wye but not 480V delta? The voltage from line to line is the same.

They are not tested for 480V delta, and the delta rating is a more difficult test. Using the breaker on a delta system would be a misapplication.

CTA-ID : 2008414
Was this helpful?
What can we do to improve the information ?