Technical FAQs

Ask a Question

What is the voltage rating for a 9422TDF60 ?

This disconnect switch has a 600V maximum rating, at which it`s rated 30 amps. At 250V it has a 60 amp rating.


CTA-ID : 2008171
Was this helpful?
What can we do to improve the information ?