Technical FAQs

Ask a Question

What are alternate aluminum lugs for 800A P frame Powerpact breakers that accept 600kcmil Al/Cu cable?

AL800P6K is an 800A 3 lug kit with each lug accepting (2) 3/0 - 600kcmil
AL800P6K4 is an 800A 4 lug kit with each lug accepting (2) 3/0 - 600kcmil
Suitable for Individually-mounted (OFF end only for P-frame) and I-Line circuit breakers per Instruction Bulletin 48049-135-03


CTA-ID : 2008157
Was this helpful?
What can we do to improve the information ?