Technical FAQs

Ask a Question

What is the maximum ampere rating of the QO panel installed in the CU12L400N, CU12L400B or CU12L400L devices.

The maximum ampere rating of the QO Panel installed in these devices is 100 ampere. The combined total handle rating of all the 2-pole Service Disconnects (QO Breakers) that can be installed on the QO panel cannot exceed 100 amperes.


CTA-ID : 2007960
Was this helpful?
What can we do to improve the information ?