Technical FAQs

Ask a Question

VC600MA5 lug kit instruction sheet 48040-344-09 kit contains two differenct types of mounting hardware. One set works and one set does not. Why does the kit contain two different types of mounting hardware?

VC600MA5 and AL800MA7 mtg screws: We have 2 different mtg screws in MA/ME lug kits becaue the kits can be used on either MA or ME brkrs. The ME brkr has clearnce holes for the mtg screw and can only use the button head screw (21605-24201).


CTA-ID : 2007961
Was this helpful?
What can we do to improve the information ?