Technical FAQs

Ask a Question

What is the thread size of the LAF/LHF terminal pad for buss connection? What is the approximate torque required?

Thread size: 3/8`` x 16 Approximate torque value: 180 lb - in.


CTA-ID : 2007952
Was this helpful?
What can we do to improve the information ?