Technical FAQs

Ask a Question

Do the two head operators, ZB4BA81**, 91** and ZB4BL81**, 91** have 2 different color buttons?

Issue:
Do the two head operators, ZB4BA81**, 91** and ZB4BL81**, 91** have 2 different color buttons?
Product Line:
22mm Push Buttons                       
Environment:
XB4 Two Head operators Momentary
Cause:
To clarify from the pictures provided in the catalog.
Resolution:
Yes. There are extra lines on the selection tables that make it look like the IP40 and IP65 versions are each one color. When actually each of the 2 head operators have 2 different color buttons.
 
Was this helpful?
What can we do to improve the information ?