Technical FAQs

Ask a Question

Do we have a part 50912-010-54 which is for a magnet controller?

50912-010-50 is the correct part number. This is a heat sink and diode assembly. The part numbe 50912-010-54 which is in bulletin #6815-16 is wrong.

The crane control portion of this business is now owned by E. C. & M. Call 1-800-240-1230 for technical support.

CTA-ID : 2007301
Was this helpful?
What can we do to improve the information ?