Technical FAQs

Ask a Question

Can a QO230GFI breaker operate on a high leg B phase system?

Issue:  
Can you use a QO-GFI breaker on a 208Y/120V system with a high-leg?

Product line:  
Residential circuit breakers

Environment:  
QO-GFI circuit breakers

Resolution:  
The GFI breakers can be used on a high-leg system, however not on the high leg.  Voltage to ground must not exceed 120Vac.  The high leg is 208V to ground.  They could connect to A and C phases.
Was this helpful?
What can we do to improve the information ?