Technical FAQs

Ask a Question

Why does the Altivar 58 not show that the frequency resolution is 0.015Hz when bit 9 of CMI (word W402) is set for 1?

This level of frequency resolution is only available with the ATV58FVC full flux vector drives. It is not available on the standard ATV58 drives.


CTA-ID : 2007064
Was this helpful?
What can we do to improve the information ?