Technical FAQs

Ask a Question

Can the LC, LI, LX, LXI, LE breakers be used with high inrush current loads, like motors?

Issue:
Motor Applications

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment

Cause:
High inrush applications

Resolution:
The application of this product with high inrush current loads such as motors/compressors shall be limited as follows:

Breaker Rating (Amps)     Maximum Full Load Current
100-400                               200
450-600                               300


CTA-ID : 2007720
Was this helpful?
What can we do to improve the information ?