Technical FAQs

Ask a Question

CKAEL36808LI What is the minimum cabinet (enclosure) space required for 100% rated breaker?

100% rated CK circuit breaker are suitable for continuous operation at 100% of rating only if used in a minimum cubicle space of H40 x W21 x D9 inches. Ventilation is not required.


CTA-ID : 2007722
Was this helpful?
What can we do to improve the information ?