Technical FAQs

Ask a Question

What quantity and size of conductors can be used on a SN225KA neutral assembly?

The SN225KA accepts (1) #4 AWG - 300 kcmil aluminum or copper conductors in and out. Two service grounding lugs each accepts (1) #14 - 1/0 AWG aluminum or copper conductor.


CTA-ID : 2007283
Was this helpful?
What can we do to improve the information ?